Building Type
70-Bed community hospital
Project Team
- Harriman Associates, Auburn, ME
- Trane
Systems Installed
- IntelliPak™ air cooled chiller
- Custom Climate Changer™ air handler
- CDQ™ desiccant wheel
Franklin Memorial Hospital (FMH) is well-known for
innovative health care. Now, FMH is first to use Trane’s
innovative CDQ™ air conditioning system—developed
with a grant from the U.S. Department of Energy.
FMH recently completed renovation of its operating
suites. Based on experience in controlling temperature
and humidity, not only for comfort requirements but for
proper operating room sterility, FMH wanted the latest in
HVAC technology. Don Garrison, chief of facility
management, said, "We always had problems being able
to satisfy the surgeons, who wanted the temperature at
62-65 degrees, while the anesthesiologists and other
staff wanted higher temperatures. It’s hard to satisfy
everyone with air that has a lot of moisture in it.”
Excessive humidity can require resterilizing surgical kits,
adding thousands of dollars of expense. Switchover to
the new HVAC system was needed in just one weekend
to avoid disrupting surgery schedules.
FMH worked with Trane and Harriman Associates
consulting engineers of Auburn, ME, to design and build
a new packaged HVAC system using Trane
components and completely assembled in
Trane’s Ft. Smith, Arkansas, factory. The
system combines an IntelliPak™ air-cooled
chiller with a Custom Climate Changer™ air
handler and a CDQ™ (Cool, Dry, Quiet)
desiccant wheel to provide superior
temperature and humidity control. The
factory-packaged system includes water
pumps, piping, Tracer Summit™ automation
system and controls.
Since the entire HVAC system was built in
Trane’s factory, changeover to the new system
was completed in a weekend. The Trane
packaged system delivers 50 degree (F) air at
35-40 F dew point, and keeps operating rooms
at 62-65 F and 35 to 50 percent relative
humidity. It delivers ideal temperature and
humidity much more efficiently than alternative
systems. Garrison says, “It’s refreshing and
rewarding to get the testimonials from the
doctors. I’ve talked to perhaps 10 of the O-R
doctors who have stopped me in the halls to
say they love the new system because it
keeps them so comfortable.”
Another example of how Trane’s
world-renowned expertise met a difficult
challenge with the right solution.
FMH is a progressive, friendly, nonprofit community general hospital whose mission is to provide
high-quality, cost-effective, patient-centered health care to west central Maine. The 70-bed hospital is
fully qualified and accredited to handle a broad range of medical, surgical, pediatric, obstetric, and
gynecological procedures and has specialized strengths in cardiology, ophthalmology, orthopedics,
otolaryngology, rheumatology, internal medicine, urology, emergency care, and occupational health.