Trane Commercial

HVAC Systems
Building Services
Controls
Products
Parts & Supplies
Educational Resources
 
Featured Case Studies
 
Energy, IAQ & The
Environment
Financing
Design & Analysis
Tools
 
TRANE FOR:
Architects
Data Centers
Department Stores
Engineers
Government
Healthcare
Higher Education
K-12 Education
Restaurants
Retail
 

Case Study - Offices and Institutions

LDS Temple Visitors Center

Download PDF | Print
LDS Temple Visitors Center

THE SPECIFICS

Expand

Close

THE SPECIFICS

Systems Installed

New, Trane Model RTWD Series R™ water-cooled chiller.

  • Series R chillers are available from 80 to 250 tons at 60 Hz and 70 to 250 tons at 50 Hz.
  • Meets ASHRAE 90.1-2007 efficiency guidelines
  • Reduced refrigerant charge and efficiency improvements to help obtain LEED certification
  • Can generate up to 140 F leaving condenser water temperature for heat recovery applications
  • Reduced sensitivity to condenser water temperatures
  • Can operate in variable primary flow applications
  • Most units fit through standard single-width door. Fork lift channels built into base for better maneuverability
  • Factory testing helps ensure trouble-free start-up
  • Adaptive Control™ algorithms provide proactive unit control and safety functions
  • Time-of-day scheduling options provide simplified unit level control
  • Easily interfaces with building automation systems with BACnet, LonTalk and Tracer Summit™ systems

Summary

New Trane Model RTWD Series R chiller installed to provide reliable, efficient air-conditioning at landmark church visitors center.

Challenge

The Trane Model RTWA Series R™ chiller installed at the Visitors Center in 1997 had accumulated more than 40,000 hours of running time—the equivalent of four and one-half years of continuous operation. Although the chiller continued to provide trouble-free operation, it was decided to replace the chiller.

Larry Packer, Manager for the Facilities Management Group at the LDS Mesa area, said, “The old chiller was running fine but it was 10 years old and had a lot of running hours. We were beginning to get concerned. We didn’t want it to go down in the middle of the summer.”

Solution

Packer hired an HVAC consultant who had done a great deal of work for the LDS Church. Packer said, “He looked at a variety of suppliers but favored Trane chillers and especially the new Model RTWD helical-rotary chiller that was going to be built in Pueblo, Colorado. Since that chiller wasn’t yet available in 2008, we delayed the replacement project about eight months until that new chiller became available.”

Results

The LDS Visitors Center received one of the very first of the new Model RTWD chillers to come out of Trane’s Pueblo factory. The new chiller was shipped in late February, 2009, and by the first week of March it was up and running, providing chilled water for the LDS Visitor’s Center.

Trent Hunt, Trane National Account Manager for the LDS Church, says the new chiller offers improved efficiency over the old Model RTWA chiller—approximately 13 percent more efficient for a projected energy cost savings of $2200 per year at the LDS Temple Visitors Center in Mesa. The new RTWD version is also significantly quieter than the old version..

Packer cited the compact size of the Model RTWD chiller that makes it ideal for replacement projects. “The installation process went very well. Sunwest Mechanical installed the chiller. It was very tight moving the new chiller into the equipment room through the door. We had only about one-half inch of clearance.”.

Jack Harris, Assistant Building Engineer, said, “We’ve been real happy with the chiller. One of our main concerns was noise because on the other side of the equipment room is a theater where we show films. You can put your ear right up to that wall in the theater and not hear a thing from the equipment room..

Harris also cited the fact that the Church has a three-year service contract with Trane that provides regular inspections and maintenance of the new chiller. Says Harris, “We’re real happy with this chiller and the service we get from Trane.” Trane

About LDS Temple Visitors Center

The Church of Jesus Christ of Latter Day Saints Temple in Mesa was completed in 1927. The Visitors Center, built in 1980, offers visitors artwork, exhibits and dioramas throughout the year—requiring an effective, efficient air conditioning system to deal with Arizona’s 100-degree plus summer weather.