Trane
Find a dealer   Make a dealer appointment
 
Products Menu
arrowIntroduction
arrowAir Conditioners
arrowCompare Air Conditioners
arrowUltra Efficiency Units
arrowSuper Efficiency Units
arrowHigh Efficiency Units
arrowStandard Efficiency Units
arrowGuide to Cooling
arrowHeat Pumps
arrowAir Cleaners
arrowThermostats
arrowFurnaces & Coils
arrowAir Handlers
arrowHumidifiers
arrowCommunicating Systems
arrowPackaged Units
arrowBoilers
arrowFrequently Asked Questions
arrowGlossary
print this page
Central Air Conditioner Efficiency Ratings: What a SEER Really Means to You

When purchasing a car, smart buyers usually check the miles-per-gallon rating.

When purchasing gasoline, they check the octane rating.

And, when purchasing a central air conditioning system, they check the SEER rating.

The what?

The SEER, or Seasonal Energy Efficiency Ratio, rating. Like its "mpg" counterpart in the automotive industry, the SEER gives an indication of the performance efficiency of the system. The higher the SEER, the more efficient the unit. And, the more efficient the unit, the lower the operating costs.

The Trane Home Comfort Institute explains that the air conditioning industry originally used an Energy Efficiency Ratio or EER to rate efficiency. This was a simple mathematical ratio of cooling output versus electrical power input.

Recently, however, the U.S. Department of Energy developed a more sophisticated test method that rates the performance of a unit over a wide range of operating conditions. The result -- the SEER -- is indicative of the unit's operation throughout an entire cooling season.

Bear in mind, however, that SEER ratings compare equipment only. Many other factors, including how you use your home and the condition of ductwork, affect energy use. That's why it's important to have a competent air conditioning dealer visit your home and evaluate your entire system.

It's also important to remember that the rating of an outdoor unit is based on a matching indoor component. As a result, if you replace an outdoor unit without replacing the indoor unit, you're not likely to get the efficiency you expect.

Experts at the Trane Home Comfort Institute say that by purchasing a system with a high SEER, you'll use less energy to cool your house, resulting in lower electric bills. In many cases, these savings are enough to partially or fully offset the cost of the new equipment within a few years.

They also recommend checking with your local utility about a possible rebate. Many utilities offer such programs based on the unit's SEER rating and cooling capacity. In most cases, the higher the SEER rating, the higher the rebate.

Finally, they point out that there's more to purchasing central air conditioning than just the SEER rating. You should also look into the reliability and durability of the system. After all, a "clunker" with good gas mileage is still a "clunker."

Your feedback matters
Your comfort is our #1 priority. Tell us how we can serve you better.
Take our Web site survey
Find Your Ideal System
Use the Trane System Customizer to choose a system based on your unique comfort requirements
Learn more
An in-depth look at air conditioners
Get more information on choosing the right air conditioner for your home.
Guide to cooling
Purchasing and financing options
See how you can work with your dealer to make your next home comfort unit a Trane.
Purchasing and financing
Why choose Trane?
Learn how quality makes all the difference for your family's total home comfort.
Clean Air is Trane Air™
The True Trane
Difference
DID YOU KNOW?
Did You Know
dyk_take_the_quiz_button.gif
See how TRANE
CleanEffects™ works
Trane Residential is a leading global provider of indoor comfort systems. Trane’s offerings include energy-efficient cooling and heating solutions for homes, air conditioners, heat pumps, furnaces, air humidifiers, thermostats, parts and service.
© 2008 Trane Inc.  All rights reserved