Trane
Find a dealer   Make a dealer appointment
 
Products Menu
arrowIntroduction
arrowAir Conditioners
arrowCompare Air Conditioners
arrowUltra Efficiency Units
arrowSuper Efficiency Units
arrowHigh Efficiency Units
arrowStandard Efficiency Units
arrowGuide to Cooling
arrowHeat Pumps
arrowAir Cleaners
arrowThermostats
arrowFurnaces & Coils
arrowAir Handlers
arrowHumidifiers
arrowCommunicating Systems
arrowPackaged Units
arrowBoilers
arrowFrequently Asked Questions
arrowGlossary
print this page
Test Your Central Air Conditioning Knowledge

If you have a quizzical look on your face whenever someone mentions central air conditioning, it's time to brush up on your knowledge of condensers and coils.

Start by taking the following quiz developed by the Trane Home Comfort Institute, a consumer information service on heating and cooling.

Answer true or false to the following statements:

1. Most central air systems are "split" systems.
2. A ton of air conditioning refers to the weight of the system.
3. Heat pumps can cool your home.
4. The higher the "SEER" of a central air conditioner, the cheaper it is to operate.
5. Price is the most important consideration when choosing a central air system.
6. The compressor is considered "the heart of the system."

When it comes to the subject of cooling, you're "hot" if you've given the following answers:

1. True. A split system means it consists of two parts: an indoor unit or coil that pulls heat and humidity from inside air, and an outdoor unit or condenser that releases that heat to the outside air. When the coil and condenser are both housed in the same unit, the system is called a packaged system.
2. False. It refers to the capacity of the system. One ton of air conditioning removes 12,000 Btu's of heat energy per hour from a home. Residential units usually range from 1 to 5 tons.
3. True. Don't be fooled by their name. Heat pumps do pump heat into your home in winter like a furnace. However, they also pump heat out of your home in summer like a central air conditioner. This ability to both heat and cool makes them very economical and efficient home comfort systems.
4. True. The SEER, or Seasonal Energy Efficiency Ratio, is an indication of the performance efficiency of the system. The higher the SEER, the more efficient the unit. The more efficient the unit, the lower the operating costs.
5. False. A recent study by the Trane Home Comfort Institute shows that homeowners rate reliability as the most important attribute to consider when selecting a central air conditioner. Purchase price ranked fifth on their list after reliability, dependability, efficiency and overall quality.
6. True. It is so called because it is the pump that circulates the refrigerant from the indoor coil to the outdoor condenser and back to the coil again. Because of its importance, look carefully at a compressor's reputation and warranty when selecting a central air conditioning system.
Your feedback matters
Your comfort is our #1 priority. Tell us how we can serve you better.
Take our Web site survey
Find Your Ideal System
Use the Trane System Customizer to choose a system based on your unique comfort requirements
Learn more
An in-depth look at air conditioners
Get more information on choosing the right air conditioner for your home.
Guide to cooling
Purchasing and financing options
See how you can work with your dealer to make your next home comfort unit a Trane.
Purchasing and financing
Why choose Trane?
Learn how quality makes all the difference for your family's total home comfort.
Clean Air is Trane Air™
The True Trane
Difference
DID YOU KNOW?
Did You Know
dyk_take_the_quiz_button.gif
See how TRANE
CleanEffects™ works
Trane Residential is a leading global provider of indoor comfort systems. Trane’s offerings include energy-efficient cooling and heating solutions for homes, air conditioners, heat pumps, furnaces, air humidifiers, thermostats, parts and service.
© 2008 Trane Inc.  All rights reserved