|
It wasn't all that long ago that, if you were in the market for a gas furnace, there
really wasn't that much to choose from.
Within the last few years, however, technological advances in gas furnace design
have given homeowners a myriad of choices, all of which are intended to increase
indoor comfort while decreasing heating costs.
The Trane Home Comfort Institute explains that regardless of the design, all gas
furnaces consist of four main components: a burner, a heat exchanger, a blower and
a vent pipe or flue.
The burner is where the gas is delivered and burned. Almost all gas furnaces today
use an electronic ignition device instead of a constantly burning pilot light to
ignite the gas.
The device works like an automobile spark plug. Whenever the thermostat calls for
heat, the ignition device instantly lights the burners. By not using any gas between
ignition cycles, this component conserves the fuel previously used by a pilot light.
The heat exchanger transfers the heat produced from the burning gas to the home's
distribution system. They come in a variety of shapes, with a serpentine configuration
being one of the most efficient and popular.
When looking at gas furnaces, the Trane Home Comfort Institute recommends that the
heat exchanger be crimped instead of welded together. The new crimped method of
manufacturing helps eliminate heat stress cracks that might occur.
The blower is a large fan that moves the heated air through ducts to the location
in the home where it is needed.
The vent pipe or flue exhausts the gaseous byproducts of combustion to the outdoors.
Depending on the type of furnace, venting can take place through the chimney or
through a plastic pipe out the side of the house.
These four components form the basis of three types of gas furnaces: a conventional
warm-air furnace, an induced draft furnace, and a condensing furnace.
Conventional warm air furnaces burn natural or propane gas to provide heat to the
heat exchanger. Indoor air flows around the heat exchanger to be heated and then
circulated throughout the house through ducts. Other ducts return air that has cooled
to the furnace to be reheated and recirculated. Additional air is drawn into the
flue for venting purposes. This air mixes with the hot exhaust gases and exits through
the chimney.
Induced draft furnaces are similar to conventional furnaces except for their venting
method. Conventional furnaces draw air through an opening in the front of the furnace
and at the flue to create a natural draft. Induced draft furnaces use a fan to draw
the combustion products into the flue. This artificially created draft increases
the efficiency of the furnace.
A condensing furnace is so named because it contains a second heat exchanger that
condenses water vapor in the hot flue gases, thereby extracting additional heat
for the home. Because the resulting flue gases are at a very low temperature, they
can be vented directly outdoors through a plastic pipe that can run through a side
wall. A drain disposes of the condensed water. Condensing furnaces are among the
most efficient on the market.
|