|
In case you don't know it, there's a whole new generation of high efficiency gas
furnaces out there that can help you cut your heating bills significantly.
With efficiency ratings over 90%, these new furnaces are designed to increase the
amount of heat obtained from every Btu of fuel you consume.
According to the Trane Home Comfort Institute, a consumer information service on
heating and cooling, the efficiency of a gas furnace is indicated by its Annual
Fuel Utilization Efficiency or AFUE rating. Developed by the U.S. Department of
Energy, the AFUE indicates what percent of the energy used is converted to useable
heat.
AFUEs for gas furnaces range from 57% to over 90%. The higher the AFUE, the more
efficient the furnace. The more efficient the furnace, the lower the heating bill.
If your present furnace is ten years old or more, it's probably in the 60-70% AFUE
range. In effect, that means you're wasting 30 to 40 cents out of every dollar you
spend for heat. By replacing an old, low efficiency unit with a new high efficiency
model, more of the fuel you pay for is turned into heat.
The Federal government now requires that all new furnaces meet or exceed an efficiency
level of 78% AFUE. It also requires that the furnaces be tested according to its
standards so that consumers can compare the efficiency ratings of various units.
The Gas Appliance Manufacturers Association (GAMA) publishes a directory of those
ratings twice a year. Your heating dealer should have a copy and can show you the
rating for the system you're considering.
The Trane Home Comfort Institute says AFUE ratings of gas furnaces have increased
over the past few years because of new furnace designs that allow the heating units
to recover heat that would have otherwise been wasted. Included among these new
designs are induced draft furnaces with AFUEs in the 80% range and condensing furnaces
with AFUEs in the 90% range.
|