Trane CleanEffects Clean Air System
The world's most effective whole-house air filtration system
Trane has always been an industry leader in home comfort. Now, we’re setting a new standard for clean indoor air with the revolutionary Trane CleanEffects™ air filtration system.
-
Trane
CleanEffects™
features
The standard air cleaners on the market have filters that are very dense. Meaning they try to stop the dust by trapping it in a slightly porous filter. The fewer the pores the more dust it can trap. However, this not only stops the dust and dirt, but it also stops the air from moving as well. In other words, the amount of air that goes through your system is reduced so you may not be as comfortable. Less air is cleaned efficiently. This is called pressure drop. The revolutionary Trane CleanEffects air filtration system has the lowest pressure drop with the highest efficiency possible. Our unique patented technology is designed to let air flow freely through the most advanced filtration system available. The result, more of your air is cleaned faster and more effectively than anything else on the market.
Trane CleanEffects utilizes patented, breakthrough air cleaning technology to remove up to an astounding 99.98% of airborne allergens from the air that passes through the filter, making it 8 times more effective than even the best HEPA room filters and up to 100 times more effective than a standard 1" filter. What's more, Trane CleanEffects has been performance-tested by LMS Technologies and Environmental Health &Engineering, Inc. (EH&E), with the results verified by professors from the Harvard School of Public Health, so you know you're getting an air filtration system like no other.
LMS Technologies is a technology consulting company that specializes in air flow measurement, filtration testing and particle analysis. Environmental Health & Engineering is an environmental consulting and engineering services company that is dedicated to ensuring safe and productive environments, and is co-founded by John D. Spengler, PhD of the Department of Environmental Health at Harvard.
-
Trane
CleanEffects™
specifics
- Removal of up to 99.98% of particles and allergens from your filtered indoor air. It removes particles as small as .1 microns – 1/1,000th the diameter of a human hair – a size that eludes most air cleaners.
- An industry-leading clean air delivery rate of 1,200.
- Low operating costs, with no replacement filters to buy.
- Cleaning indicators easily visible on the outside of the unit.
- Easy to clean filters—just vacuum or rinse once every 3 to 9 months (depending on usage).
- Easy installation.
- Quiet operation
- Trane CleanEffects was designed to fall well below the 50 parts per billion (ppb) FDA voluntary emission limit for medical devices. Trane CleanEffects contributes a negligible amount of ozone – less than .3 ppb to the living space.
- To put this into perspective further, typical ozone levels during the summer outdoors are at about 60 to 90 ppb, and indoor levels can vary greatly but are typically between 12 ppb to more than 80 ppb. Testing of Trane Clean Effects by third parties has shown there’s no more ozone in a home installed with Trane CleanEffects than naturally occurs in the environment already
- Trane CleanEffects is the industry benchmark supported and verified by third parties who make it their business to know about clean air. Experts from LMS Technologies, EH&E, Harvard School of Public Health and other major university research shows Trane CleanEffects to be the best air filtration system on the market.
- Low pressure drop.
-
Trane 10-year limited warranty details
- Trane CleanEffects has a ten-year limited warranty on the system’s electronics, and a five-year parts limited warranty on the system filters.
- Extended warranties are available for Trane CleanEffects and also the rest of your Trane system. Ask your installing dealer for details.
Links
Save on your system this spring
36 Month No Interest* or 3.9% APR* or Up to $1,000 Rebate*




Search for a Trane Comfort Specialist dealer in your area.