We use cookies to enhance your experience on our website. By clicking '' or by continuing to use our website, you are agreeing to our use of cookies. You can change your cookie settings at any time.
het pumps m

Advanced HVAC that's Electrifying

Engineered to maximize comfort and minimize energy use. For HVAC, this is pretty exhilarating stuff. Upgrade with a Trane heat pump system and start saving today.*

Upgrading to a more energy-efficient Trane heat pump system can be fun! Okay, maybe not “fun.” But it can save you energy and dollars.

dollar sign trane red  1  1

Heat pumps can save
homeowners up to

40%

on heating and cooling costs1

Heat pumps transfer heat from one location to another and this energy-efficient heating can help save money.

efficiency trane red  1  1

Seasonal Energy Efficiency Rating
(SEER2)

16+

indicates energy efficiency

Choosing a heat pump with a SEER2 rating of 16 or more can improve efficiency, lower energy bills, and reduce your carbon footprint2.

in home mode

Heat pumps can reduce
greenhouse emissions by up to

50%

compared to traditional HVAC systems3

Heat pumps are an electric option for heating and cooling homes that use less energy and provide consistent year-round performance.

There is a closeup of a Trane air unit.

Save with offers, rebates, and incentives

Good news for homeowners!

Recent legislation changes mean that upgrading your HVAC system may not only save you energy, but also earn you tax credits and rebates. The Inflation Reduction Act (IRA) has allocated nearly $370 billion towards climate and energy programs, with incentives for energy-efficient purchases as a major focus.

Enjoy annual tax credits as a homeowner from January 2023 to December 2032, regardless of your income level. Savings are available nationwide and include:

  • Up to $2,000 for qualified Heat Pumps
  • Up to $1,200 per year for qualified expenditures including:
    • $600 for qualified furnaces
    • $600 for electrical upgrades to enable heat pump installations
    • $600 for qualified air conditioners

Maximum tax credit is $1,200/year or $3,200/year if expenditures include a qualifying heat pump.

Tax credits and rebates near you

Use the search field below to discover available tax credits and rebates for heat pump systems. And when you're ready, talk to an expert.

in home mode

10M+

Trane units in households

Our customers expect reliability
and innovation built into their
HVAC comfort.

verified user

2,600

Hours of testing

Trane makes systems you
can rely on for years to come so you
have comfort when you need it most.

account circle

10K

Trane Dealers

Dealers stay up to date on the
latest technology to provide fast,
reliable HVAC service.

Lifestory Research America's Most Trusted HVAC Brand 2015 - 2025
Trane received the highest numerical score in the proprietary Lifestory Research 2025 America's Most Trusted® HVAC Brand study. Study results are based on experiences and perceptions of people surveyed. Your experiences may vary. Visit www.lifestoryresearch.com

1U.S. Department of Energy Efficiency & Renewable Energy. Heat pumps can save homeowners up to 40% on their heating and cooling costs compared to traditional HVAC systems. Visit energy.gov/energysaver/heat-pump-systems for more info.

²U.S. Department of Energy (DOE). New M1 testing procedures provide a more thorough and accurate assessment of HVAC system testing. Choosing a cooling system with a higher SEER rating, especially SEER 16+ can improve energy efficiency, lower energy bills, and reduce carbon footprint.

3U.S. Environmental Protection Agency and Department of Energy. “Heat Pump Systems.” Today’s heat pump can reduce electricity use for heating and reduce greenhouse gas emissions by up to 50% compared to traditional HVAC systems. Visit energy.gov/energysaver/heat-pump-systems for more info.

*Enjoy annual tax credits as a homeowner from January 2023 to December 2032, regardless of your income level. Savings are available nationwide and include tax credit savings depending on the HVAC system purchased. See your participating independent local utility for complete program details, including eligibility, restrictions, and effective dates. Local utilities will determine final rules regarding participation, rebate submissions, and payouts. Offers may have different effective dates, subject to local utility discretion. Offers are valid on Qualifying Equipment only.

**America’s Most Trusted®: Trane received the highest numerical score in the proprietary Lifestory Research America’s Most Trusted® HVAC Brand study for years 2015-2025. Study results are based on experiences and perceptions of people surveyed. Your experiences may vary. Visit www.lifestoryresearch.com. America’s Most Trusted® HVAC Brand 9 Years in a Row.