A gas furnace uses gas as a fuel source to produce heat, which is then re-distributed throughout your home.
A gas furnace is a type of heating system that utilizes natural gas or propane to generate warm air. This air is then pushed through ductwork and distributed throughout the entire home, ensuring even temperatures in each room. Gas furnaces are energy efficient, cost-effective and easy to operate; they produce more heat for less money than other types of central heating systems.
Gas furnaces use an ignition source (such as electric spark) to ignite the gas as it enters the burner assembly. This ignites the mixture of fuel and air, creating combustion which produces heat. The heat is then transferred into metal chambers where it radiates from hot surfaces within the unit before being blown into the home’s air distribution system. The blower fan within the furnace then distributes the warm air through the ductwork until all rooms of the home are evenly heated. Watch a video to learn how a furnace, heat pump, and AC work together.
Gas furnaces are one of the most efficient and cost-effective heating systems available today. Additionally, gas furnaces have longer lifespans than other types of heaters, typically lasting anywhere from 20-30 years depending on usage and maintenance. Other benefits include:
If you’re looking for an efficient and cost-effective way to heat your home, a gas furnace may be the perfect solution. Contact your local Trane Comfort Specialist today to learn more about how a new Trane gas furnace can help keep your family warm this winter.
Furnaces are a whole-home heating solution that work by burning a fuel source, like natural gas or propane, to make heat. The heat produced is combined with cold air from your home, then is re-distributed via ductwork to increase indoor temperature.
An oil furnace uses oil as a fuel source to produce heat, which is then re-distributed throughout your home to increase the temperature.
Dealers can answer questions, help you find the right products for your home, and repair your system.
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone