We use cookies to enhance your experience on our website. By clicking '' or by continuing to use our website, you are agreeing to our use of cookies. You can change your cookie settings at any time.

Pleated Filter

Pleated filters are a type of filter that will be found in an air duct or in a furnace or air handler to trap particles like dust and dander and prevent them from circulating in your home.

What is a pleated filter?

Pleated filters are made from pleated cloth or paper that is pleated or folded in a series of small pleats, which help to increase the filter’s surface area and capture more particles. This type of filter is often used in air conditioning systems, air purifiers, and other indoor air quality devices. Filters help keep the HVAC clean so it continues to operate at peak performance. Without a filter, debris will settle onto the fan and coils which over time will restrict airflow and performance. Pleated filters are one of the most popular types of filters on the market because they can trap a large amount of particles and keep them from contaminating your home. 

Benefits of pleated filters

Pleated filters offer several benefits, including: 

  • Increased surface area: The pleating creates a larger surface area allowing these filters to capture more particles and provide better overall filtration.
  • Better filtration performance: pleated filters are designed to trap smaller particles, making them ideal for capturing allergens like pollen and pet dander. Additionally, pleated filters have a higher capacity for trapping pollutants, so you’ll get cleaner air in your home with less frequent filter changes. 
  • Long lasting: modern pleated filters are relatively long lasting, so you won’t need to replace them as often. This helps save money in the long run and keep your indoor air quality consistently high over time.

What are other types of filters?

While pleated filters are the most common type of filter, there are other types of filters available. These include carbon filters, electronic air cleaners, and more. Each has its own unique features and benefits that might make it a good option for your home. It’s important to do your research before choosing a filter so you can find one that fits your needs.

Choosing a pleated filter for your home

When it comes to choosing a pleated filter for your home, there are several factors to consider. First, you’ll want to make sure that you choose a pleated filter with the right MERV rating for your needs. The Minimum Efficiency Reporting Value (MERV) ratings runs from 1-16 and indicates how effective a pleated filter is at trapping particles of different sizes – the higher the MERV rating, the better it is at trapping smaller particles. EPA recommends using the highest MERV rated filter your system can handle.

You’ll also want to make sure that your pleated filter is compatible with your existing HVAC system or air purifier. All in all, pleated filters can offer a great solution for improving your indoor air quality. With the right MERV rating and an appropriate filter size, pleated filters can help reduce allergens, dust mites, pet dander and other pollutants from entering your home or office. 

Shop Trane air purification systems

Contact a local dealer

Dealers can answer questions, help you find the right products for your home, and repair your system.

We’re here to help

Connect with our Customer Care team about your products, warranties, and dealer concerns.

Available Monday – Friday from 7am to 5pm CST

1-833-298-3493

A phone