We use cookies to enhance your experience on our website. By clicking '' or by continuing to use our website, you are agreeing to our use of cookies. You can change your cookie settings at any time.

Refrigerant Reclamation

By Anne Fonda

In the case of HVAC refrigerants, reclamation means reclaiming the refrigerant to restore it for use again. This process starts with refrigerant recovery, where the refrigerant is removed from an air conditioner or heat pump. 

The American Society of Heating, Refrigerating, and Air-Conditioning Engineers (ASHRAE) has several definitions very specific to refrigerants that apply.

Recover

To remove refrigerant in any condition from a system and store it in an external container.

Recycle

To reduce contaminants in used refrigerants by separating oil, removing noncondensables, and using devices such as filter driers to reduce moisture, acidity, and particulate matter.

Recycled Refrigerants

Refrigerants for which contaminants have been reduced by oil separation, removal of noncondensable gases, and single or multiple passes through filter driers or other devices that reduce moisture, acidity, and particulate matter.

Reclaim

To process used refrigerant to new product specifications.

Reclaimed Refrigerants

Refrigerants reprocessed to the same specifications as new refrigerants by any means, including distillation. Such refrigerants have been chemically analyzed to verify that those specifications have been met.

Why Does All of This Matter?

Refrigerants can cause harm to the environment if not handled properly. If your HVAC system has a refrigerant leak or you’re getting a new system, your HVAC technician needs to be skilled in this area.

When Does Refrigerant Recovery Happen?

There are two situations where refrigerant recovery happens. The first is during some air conditioning repairs involving the refrigerant lines. Second, recovering the refrigerant from an older system is also necessary during air conditioner replacement. We will also include heat pumps in this scenario because they use refrigerant to cool and heat your home.

Depending on the age of your residential cooling equipment, this process will involve R-22 recovery (Freon® recovery) or R-410A recovery. There are other refrigerants, but these are the most common for residential HVAC systems. 

How Refrigerant Recovery Works

For your safety and the planet’s health, only a trained HVAC professional with the appropriate certification under Section 608 of the Clean Air Act should perform refrigerant recovery.

They will use specialized refrigerant recovery equipment to perform the job safely. After ensuring all valves are closed, they will connect special hoses to the condenser unit, which connect to a manifold. Hoses on the other side of the manifold connect to a refrigerant recovery machine, and finally a refrigerant recovery cylinder.

At the beginning of the process, all the valves are closed. During the recovery process, the technician opens the valves, allowing the refrigerant to exit the cooling unit, go through into the recovery machine, and then out the other side into the recovery tank.

Multiple Techniques

There are multiple ways to recover refrigerant. The technician will choose a technique based on your system, the volume of refrigerant to be recovered, and more.  Once they have safely removed the refrigerant, they can make the necessary repairs to your refrigerant lines. Or, they can safely disconnect the old unit and install a new condenser unit.

They then have two choices – recharge the refrigerant in the unit that just underwent repairs, or recycle the refrigerant at an HVAC supply location that accepts recovered refrigerant. Recycling would be the choice when you install a new AC unit or heat pump – new split system cooling units come pre-charged from the factory. 

Why HVAC Refrigerant Recovery, Recycling, and Reclamation is Important

Properly completed refrigerant recovery prevents the environmental impact of improper refrigerant disposal. A release of 1 lb of R-410A = 1 ton of carbon dioxide from a global warming perspective.

Environmental Protection Agency (EPA) regulations forbid intentional refrigerant venting for this very reason. HVAC technicians must properly remove refrigerant from AC units and heat pumps when necessary for HVAC repairs or HVAC replacement. They are then required to safely recharge a unit after repairs, or recycle the refrigerant.

Have refrigerant questions? Contact your local Trane dealer for expert advice.

Anne Fonda, Content Writer

LinkedIn

A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.

She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism.

When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.

Expert review by Steve Kujak, Director Next Generation Refrigerant Research

Contact a local dealer

Dealers can answer questions, help you find the right products for your home, and repair your system.

We’re here to help

Connect with our Customer Care team about your products, warranties, and dealer concerns.

Available Monday – Friday from 7am to 5pm CST

1-833-298-3493

A phone

What do you need help with?