Two-stage heating means your furnace functions at two levels of heating output, depending on the temperature outside.
Two-stage heating means your unit functions at two levels of heating output, depending on the temperature. Two-stage heating is an energy-saving feature found in many furnaces and heating units. It’s designed to work two ways: in colder weather, the two-stage heating system typically runs at high output, working hard to keep your home warm and comfortable; on milder days, the two-stage system can run at a lower output for greater efficiency.
This two-part system maximizes your energy savings, as you won’t be paying to heat your home to an unnecessarily high temperature on milder days.
One-stage heating systems are the more traditional model. They run at a constant output, regardless of your home’s heating needs. This means that on mild days, you may be paying to heat your home more aggressively than needed, or to an unnecessarily high temperature. Two-stage heating systems are designed to address this issue, as they adjust their output depending on how close the current temperature is to the desired temperature. You can also watch this video to learn the difference between variable speed, two-stage, and single-stage HVAC systems.
There are several benefits that come with two-stage heating systems:
Two-stage heating is an excellent way to maximize efficiency and save money on your energy consumption. With two different stages of output, it’s designed to keep your home comfortable while minimizing costs in warmer months. If you’re looking for a more efficient and economical alternative for heating your home, two-stage heating could be the ideal choice for you.
Furnaces are a whole-home heating solution that work by burning a fuel source, like natural gas or propane, to make heat. The heat produced is combined with cold air from your home, then is re-distributed via ductwork to increase indoor temperature.
Single-stage heating refers to a furnace or other heating unit that has one level for heat output, regardless of the temperature outside. This is different from some other systems that have more than one speed, and can operate on a high stage or a lower stage depending on how much heating is needed to keep your home comfortable.
Dealers can answer questions, help you find the right products for your home, and repair your system.
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone