By Anne Fonda
Bioaerosols are microorganisms, particles, or fragments of biological origin, meaning they are either alive or came from a living organism that are in the air. Bioaerosols are everywhere in the environment.
Measured in microns, they range from .05-100 microns (symbol µ). They are small enough to be inhaled. Examples of household bioaerosols include:
These bioaerosols, or contaminants, affect your indoor air quality (IAQ) and can affect your health.
How do bioaerosols affect human health? In a nutshell, they can cause both hypersensitivity illnesses and Infectious diseases.
These are more commonly known as allergic illnesses or allergic responses. Some people are more sensitive to certain allergens, which can trigger the body’s autoimmune response.
Examples and associated symptoms include:
While less commonly occurring in a residential environment, certain bioaerosols can cause infectious diseases. Examples include:
Pontiac fever is marked by fever, body aches, headache, cough, and shortness of breath without pneumonia. It’s caused by the same bacteria that causes Legionnaire’s disease.
Your home’s HVAC system can provide a defense against bioaerosols. A standard 1” HVAC air filter can filter out some contaminants but to capture smaller particles and to flush contaminants out of your home, you may want to consider additional HVAC equipment.
Beneficial systems include:
Whole-house air cleaners/air purifiers such as the Trane CleanEffects® Whole-House Air Cleaner and QuikBox® Air Cleaner use advanced filtration technology to capture bioaerosols and other allergens and particulate matter as small as .3-1 microns. Learn more about each of these systems in our Trane’s Best Air Purifiers article.
While the systems can greatly reduce contaminants such as fungi, viruses, and bacteria, they cannot completely remove them.
Some contaminants/bioaerosols, such as bacteria, can thrive in conditions with inadequate ventilation. Your central heating and air conditioning units alone don’t mechanically bring fresh air in from the outdoors – they simply recirculate the indoor air. However, ventilation systems such as a whole-house ventilator bring fresh air in and remove stale indoor air. They circulate air to help remove some bioaerosols.
Bioaerosols such as mold and dust mites thrive in high-humidity environments. High humidity is considered to be anything at or above 60% relative humidity. While bathroom exhaust fans can help regulate the humidity in your bathroom, if you have high humidity in your whole house, you need a whole-house solution.
A whole-house dehumidifier can be a great solution if you live in a humid climate or have a single-stage AC unit that sometimes has a hard time removing moisture from the air.
Contact your local Trane Comfort Specialist for a consultation and product recommendations tailored to your home and family.
Anne Fonda, Content Writer
A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.
She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism.
When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.
Expert review by Jennie Bergman, Senior Product Manager, Indoor Air Quality
A micron, or micrometer, is a very small unit of measure equal to one millionth of a meter. Airborne particles such as dust, smoke, dander, or bacteria are often a few microns or less and can only be captured by an indoor air cleaning system.
An HVAC air purifier is an air cleaning unit that connects to your home’s HVAC system. Also known as an air cleaner, air purification systems vastly improve your indoor air quality.
Learn about indoor air quality – what it is and how to improve it for your family’s health and the health of your HVAC system.
Dealers can answer questions, help you find the right products for your home, and repair your system.
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone