The condenser coil is one of two coils found in your cooling system that work together to complete the heat exchange cycle. The condenser coil is located outside the home, and it’s where the refrigerant releases the heat it absorbed from inside.
A condenser coil is one of two coils found in your cooling system that work together to complete the heat exchange cycle. The condenser coil is located outside the home, and it’s where the refrigerant releases the heat it absorbed from inside. It is responsible for rejecting the energy taken up by the evaporator coil into an external environment, usually an outdoor air source. This heat exchange process creates cool air which then circulates back through the HVAC system throughout your home.
The size and shape of a condenser coil can vary depending on its intended application, but in most systems you will typically find a large metal shell with rows of tubes running vertically or horizontally within it, each containing finned aluminum coils. These fins are specifically designed to help increase the surface area of the condenser coil, allowing it to reject more heat faster and more efficiently.
The condenser coil plays an important role in the operation of your system. Without a properly functioning condenser coil, your system would not be able to keep up with cooling demands or maintain comfortable temperatures inside your home. It also helps reduce operational costs by improving energy efficiency since it releases more heat into external environments rather than back into your living space.
Additionally, air conditioning systems with larger coils can offer increased cooling capacity and improved seasonal energy efficiency ratings (SEER2). In short, having a well-maintained condenser coil is essential for efficient long-term operation of your system.
To ensure the best possible performance from your condenser coil, it is important to keep it clean and free from debris. While maintenance should only be handled by a licensed HVAC technician, you can also regularly inspect the area around your unit for any obstructions like tall grass or shrubs that could inhibit air flow.
Because the internal components and fins on the coil may accumulate dirt and dust over time, which can reduce airflow and cause inefficient cooling, it’s a good idea to schedule regular cleaning and maintenance. Contact a local Trane technician for help.
Air conditioners remove heat and humidity from the air in your home and place it outside to reach your desired indoor temperature. Central AC cools your entire home, while ductless AC cools just one portion or room in your home.
The evaporator coil is the component of your heat pump or air conditioner that absorbs heat and moisture from the air inside your home. It then works with the condenser coil to produce cool air and complete the heat exchange cycle.
Dealers can answer questions, help you find the right products for your home, and repair your system.
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone