A basic compressor definition is that it’s a mechanical device that increases the pressure of a gas or air by decreasing its volume. An HVAC compressor is a vital component in your cooling system.
An HVAC compressor is either an AC compressor or a heat pump compressor. Most people call them air conditioner compressors or air conditioning compressors, but in reality, the compressor in your heat pump (HP) is virtually identical. All Trane heat pumps and AC units use the patented Climatuff™ compressor.
Your heat pump or AC compressor is the lifeblood of your outdoor unit. The compressor is responsible for circulating and pressurizing the refrigerant in your unit, so the refrigerant can carry and release heat. If refrigerant didn’t move throughout your unit and release heat, cold air wouldn’t be produced and your home would remain warm. This means, that without the compressor, your unit wouldn’t be able to function.
Refrigerant is a cooling compound that absorbs heat and humidity from your home, carries it, and then releases that heat and humidity outside to ultimately cool your home. In heating mode, a heat pump reverses the refrigeration cycle to transfer outdoor heat energy into your home. But, the refrigerant can’t do its job without the compressor.
Refrigerant changes from liquid to gas during its journey through the air conditioner, but when it reaches the compressor, it is in gaseous form. The compressor applies energy to the gaseous refrigerant or compresses it, so it becomes a high-pressure gas. The compressor also raises the temperature of the refrigerant, so that it’s hotter than the temperature outside.
Once the compressor performs these two tasks on the refrigerant, the refrigerant is forced into the condenser coil. Here, it can release all the heat and humidity it’s carrying outside and turn back into a liquid.
Your HVAC compressor is one of the hardest working parts of your AC system or heat pump system. All that wear and tear can lead to an eventual breakdown. You should know a compressor can also be one of the most expensive parts to replace.
If your air conditioner compressor fails, your entire air conditioning unit will fail, resulting in the need for AC troubleshooting. An HVAC compressor carries a high voltage so improper handling can result in serious injury or death. Therefore a licensed HVAC technician is the only person to inspect and service a broken compressor. But there are some warning signs of compressor failure, including, but not limited to:
Without getting too close to your unit, stand near the outdoor fan. Without actually touching the unit, align your hand with the fan. You should be able to feel a stream of hot air coming out of the unit. If you feel lukewarm or cold air coming from the unit in the summer, your compressor might not be working.
If you suspect that your heat pump or AC compressor might be failing, you’re likely wondering if you should repair or replace the unit altogether. The first step in this process is to bring in an HVAC contractor to ensure it’s your compressor that has failed and that no other parts of your air conditioning system or heat pump system are causing issues.
After that, here are some things you should consider when you’re thinking about whether you should repair your air conditioner compressor or replace the entire unit:
Check out our Repair or Replace Guide to help you make this important decision.
How much it costs to replace your heat pump or AC compressor depends largely on whether your unit is under warranty or not. If your unit is under warranty, the cost of the compressor itself would likely be covered, but you would be responsible for labor costs.
If it’s not under warranty the compressor replacement can cost anywhere between $900-$2,900, according to Forbes.
Keep in mind, that sometimes it might be more cost-effective to replace your unit entirely if your compressor doesn’t work, especially if your unit is not under warranty. Federal tax credits and heat pump rebates make now a more affordable time to upgrade your HVAC system.
Compressor maintenance is NOT a DIY project. Compressor maintenance should only be handled by an HVAC professional. The main things you can do yourself to maintain your heat pump or AC unit are to make sure nothing is on top of or blocking the unit that might restrict airflow, and to regularly change your air filters.Beyond that, heat pump or air conditioner maintenance is to be handled by an HVAC professional. When your technician services your unit, they’ll make sure your compressor and the rest of your unit is running properly. They’ll also clean your condenser coil, which works hand in hand with the compressor to release hot air. With proper maintenance, the HVAC compressor can last up to 15 years!
The Trane Climatuff™ is the world’s first successful heat pump compressor, and it is the type of compressor found in all Trane residential units.
Refrigerant is a chemical cooling compound that absorbs and releases heat at different points in the heat exchange cycle as it runs throughout an HVAC system.
Learn about the refrigerant cycle and how your Trane heat pump or central AC system cools your home.
Dealers can answer questions, help you find the right products for your home, and repair your system.
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone