By Anne Fonda
A thermostatic expansion valve (TXV) is a small HVAC part that plays a big role in air conditioning systems. This valve regulates the flow of refrigerant entering the evaporator in the refrigeration cycle. An outdoor AC unit will have one TXV, but a heat pump may have two – one each for the cooling and heating cycles.
The TXV valve is located near the indoor evaporator coil (“A” coil). There is a sensing bulb connected to the gas line leaving the evaporator. It creates a feedback loop to increase or decrease the mass flow through the TXV to regulate superheat. This protects the compressor from flooding or overheating. The sensing bulb relies on contact with the gas line leaving the evaporator to accurately sense the temperature of the refrigerant leaving the evaporator and adjust accordingly.
The sensing bulb is connected to the TXV by a capillary tube so it can create a force balance with the other inputs to the TXV. This helps the evaporator operate most efficiently to cool your home. In addition, by regulating refrigerant flow, pressure, and evaporation, the TXV protects the compressor and helps it achieve optimal performance.
An electronic expansion valve (EEV) is a more sophisticated, industry-leading, technically superior refrigerant metering device. It more precisely controls the refrigerant flow to the evaporator. EEVs control the flow of refrigerant in response to signals from an electronic controller which electronically opens and closes a needle valve.
Trane cooling systems use an electronic expansion valve rather than thermostatic expansion valves because the technology is best in class.
Troubleshooting and maintenance of the TXV or EEV should only be done by a trained HVAC technician. During annual air conditioner maintenance, they will inspect the valve, associated components, and the rest of your cooling system parts.
They will clean parts as needed, check for refrigerant leaks, and more, to help ensure your system operates at peak performance.
When your air conditioner or heat pump is properly maintained, the TXV or EEV system can last for the life of the AC unit or heat pump. If your AC is blowing hot air, the evaporator coil freezes, or you have fluctuating temperatures, a failing thermal expansion valve could be to blame. Call in an HVAC professional to find the problem.
Whether you need AC repair, HVAC maintenance, or HVAC system replacement, work with the HVAC professionals you can trust. Contact your Trane local HVAC dealer today for all your HVAC needs.
Anne Fonda, Content Writer
A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.
She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism.
When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.
Expert review by Kimberly Sexton, Senior Systems Engineer
Learn about the refrigerant cycle and how your Trane heat pump or central AC system cools your home.
Refrigerant is a chemical cooling compound that absorbs and releases heat at different points in the heat exchange cycle as it runs throughout an HVAC system.
Dealers can answer questions, help you find the right products for your home, and repair your system.
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone