HVAC Troubleshooting
Follow our interactive troubleshooting guide to find answers to your system’s problems.
Choose from a selection of common HVAC issues or pick your product for help with fixes you can try yourself.
Do Mini-Splits Have Filters, and How Do I Care for Them?
Yes, mini-splits have filters. If you have a single-zone or multi-zone ductless mini-split system, you know how great they are for heating and cooling your home, giving you full control of the temperature in each room or zone. To keep your system functioning at peak performance, you must care for the filters properly.
Similar to a window AC unit or wall unit, mini-split AC units and ductless mini-split heating and cooling indoor units have reusable and washable filters. With careful handling, Trane/Mitsubishi mini-split filters are made to last up to 10 years. Should you need a mini-split air filter replacement, contact your ductless system installer.
Trane/Mitsubishi mini-split air filters vary based on the indoor unit - they may have multiple filters. Some options include:
- Standard air filter
- Nano platinum filter
- Electrostatic anti-allergy enzyme filter
- High-efficiency filter
- Air-purifying filter
- Long-life filter - available in ceiling-mount mini-splits - these cassette mini-splits may also have a filter check signal
Refer to your owner's manual for additional details.
How often mini-splits need to be cleaned will depend on the unit. You should perform Trane/Mitsubishi mini-split filter cleaning according to your owner’s manual. That can be as often as every two weeks during peak heating or cooling season. You may be OK with cleaning the filter once a month during less frequent usage. Refer to your owner's manual for specific instructions for your system.
You can dust or wipe down the exterior of your indoor units as part of your regular cleaning schedule. Keep the outdoor unit clear of debris or snow, and keep shrubs and plants trimmed at least two feet away from the unit.
How to clean a Trane/Mitsubishi mini-split filter
If you have a Trane/Mitsubishi mini-split, here is how to clean the air filters. Remember, not all units are the same, so check your owner’s manual for directions as well. They may differ slightly from these.
- Turn off the mini-split at the wall control or with the remote control.
- Open the unit by lifting up/pulling down the front panel.
- Gently lift the air filters out, being careful not to shake off dust during removal. (Or you’ll need to clean that up later.)
- Unclip the smaller filter from the larger one. Set it in a safe place. These smaller filters should not be allowed to get wet.
- Vacuum and/or rinse the large air filters. Using a brush attachment and low suction, vacuum the filters. Suction that is too strong can damage the filter.
- You can also gently handwash the filters in your sink. Use lukewarm water and the spray attachment on your faucet for best results.
- Allow the air filters to thoroughly dry.
- Once the filters are completely dry, snap the smaller deodorizing filter back on.
- Gently slide the larger air filters back into the mini-split.
- Close the panel.
- Turn the power to the mini-split back on.
Repeat the process for additional units. For further guidance, refer to your owner’s manual. If you have difficulty, your HVAC company can assist you.
Keep up with the mini-split filter cleaning schedule to help prevent problems with your ductless system. Clogged filters can cause
- Poor or no cooling
- Poor or no heating
- Water leakage
- Mold and mildew issues
- Musty smell
- System damage
Schedule professional ductless HVAC maintenance at least annually. Twice a year is better if you have a ductless mini-split heating and cooling system. During the maintenance visit, the HVAC technician should:
- Thoroughly inspect and clean the units
- Check for refrigerant leaks
- Check electrical connections
- Provide mini-split air filter replacement for old or damaged filters
- And more
Be sure to work with an HVAC company experienced with mini-split units - preferably the company that installed your system. Consider signing up for a service contract so you don’t forget to schedule maintenance.
Anne Fonda, Content Writer at Trane Technologies
A Content Writer with Trane Technologies, Anne Fonda researches topics and writes for Trane® and associated residential HVAC brands. She works in collaboration with Trane Technologies subject matter experts, offering easy-to-understand, informative content on complex topics. Her goal is to help consumers make informed decisions on the products and services they need.
She has written for HVAC and other service provider websites for over 16 years. Before transitioning to web content writing, Anne had a 14-year stint as an award-winning journalist. She graduated cum laude from the University of Missouri-Columbia School of Journalism. When she’s not working, Anne enjoys playing word games, reading, gardening, spending time with family, and visiting gardens and museums.
Expert review by Kimberly Sexton, Senior Systems Engineer
Is your HVAC system still experiencing issues?
Your local Trane dealer can help.Maintenance Tips
A healthy HVAC system can last longer and save money. Maintain your system with these tips.
Owner’s Manual
Learn more about your product, like its technical specs and innovative technology.
Warranty & Registration
After getting a new system, be sure to protect it with a warranty.
Contact a local dealer
Dealers can answer questions, help you find the right products for your home, and repair your system.
We’re here to help
Connect with our Customer Care team about your products, warranties, and dealer concerns.
Available Monday – Friday from 7am to 5pm CST
A phone