Comprehensive Chilled Water Systems

Enhance building efficiency with Trane chilled water systems

Overview

State of the art chilled water system design.

An integrated approach to applied mechanical system design can help lower the power draw, allowing the entire system to operate more efficiently with less money and less energy. 

  1. Reduce Lifecycle Costs

    Chilled water systems leverage chiller efficiency, improved flow rate designs, and high-performance equipment selections to minimize lifecycle costs.

  2. Ultimate Flexibility & Reliability

    Building load changes are managed by pairing chillers with a wide range of airside equipment, using pre-engineered chiller plant control sequences that respond to fluctuations in cooling loads.

  3.  Sustained High Performance

    System design uses advanced components to deliver high performance over time by maintaining proper delta T and peak chilled water system efficiency.

Product Information

Comprehensive Chilled Water Systems include chillers, cooling towers, condenser-water pumps, chilled-water pumps, and hydronic terminals with control valves. Featuring fixed- or variable-speed compressors, our systems meet or exceed energy code requirements and offers centralized equipment for easy maintenance.


  • CenTraVac CDHH Background

    Water-Cooled Chillers

    A diverse portfolio of water-cooled chillers, featuring centrifugal and helical rotary screw technologies, ranging from 200 to 6,000 tons.

  • Trane® Ascend® Air-Cooled Chiller model ACX

    Air-Cooled Chillers and Heat Pumps

    Trane’s air-cooled chillers and heat pumps are designed for customizable efficiency, sustainability, and cost-effective thermal management in commercial buildings.

  • Thermafit Modular Air-Source Multi-Pipe model MAS

    Thermafit™ Modular Chillers

    Trane’s line of Thermafit™ modular chillers and heat pumps create operational redundancy without compromising performance, sustainability and efficiency.

  • energy-storage-solutions-1400x600-web-banner.jpg

    Thermal Energy Storage

    Behind-the-meter load flexibility helps building owners and facility leaders increase energy cost resiliency and sustainability. Trane Energy Storage Solutions provide the flexibility needed to focus on your core business.

  • Ensemble on a Desktop

    Building Control Solutions

    Enhance your buildings performance with Trane’s innovative building control solutions, designed for both modern and previous systems to improve comfort and reduce energy consumption.

  • Air Heating and Cooling Coil large wide model 1

    Cooling Coils and Heating Coils for Air Handlers

    Trane cooling coils and heating coils for air handlers are optimized for a range of pressure drop and capacity requirements.

    Learn More

Easy to Understand Controls

By applying advanced technology and controls, state-of-the-art doesn’t mean high complexity or difficult algorithms. Trane delivers project-ready automation designs and collaborates with you from design to implementation.

CenTraVac® Water-Cooled Centrifugal Chillers

Trane CenTraVac centrifugal chillers deliver high-capacity, energy-efficient thermal management for a variety of application challenges. Their advanced features help reduce operational costs and environmental impact.

Product Literature

FAQs

Your questions about comprehensive chilled water systems, answered.

Comprehensive chilled water systems are a high performance and reliable centralized cooling solution that circulates cold fluid through pipes, coils and valves to extract heat from the building.

A chilled water system cools water using a chiller, then pumps it through a network of pipes to absorb heat from the building via cooling coils. The coils use chilled water to cool the air, which is then distributed to maintain comfortable and consistent indoor temperatures.

Trane chilled water systems feature high efficiency chillers with various compressor options, hydronic accessories including pumps, coils, and valves, and advanced control systems. Additionally, these systems incorporate cooling towers, control sequences, and digital services for remote monitoring.

Resources & Insights

Explore the latest comprehensive chilled water system resources.

  • Sullivan County Courthouse
    • Customer Story & Case Study

    Sullivan County Courthouse

    Trane upgraded Sullivan County Courthouse's aging systems, enhancing efficiency and comfort, and reducing energy costs. The project was timely and within budget.

  • EdmondsCommunity_College-Page.jpg
    • Customer Story & Case Study

    Edmonds Community College

    Founded in 1967, Edmonds Community College helps students access educational and career opportunities in a supportive environment that encourages success, innovation, service and lifelong learning. The college spans fifty acres in the heart of a northern Seattle suburb and employs more than 1,600, contributing to the vitality of state and local economies. Edmonds has 21,000 students enrolled in Associate’s Degree programs, career training, adult literacy, or continuing education classes.

  • CrosstownConcoursePart2.jpg
    • Customer Story & Case Study

    Crosstown Concourse - Part 2

    The Crosstown Development Team wanted its abandoned building to serve as a catalyst for growth in the arts, education and healthcare in an under-served area of Memphis. This team knew that creating a financially and environmentally sustainable “vertical urban village” would play a key role in revitalizing the neighborhood. They established a series of strategic goals to increase value for property owners, including: lowering operational costs, promoting sustainability, and maximizing asset potential. The group sought the resources of a strategic partner to align with them in building this community.

  • One Clearlake Centre hero.jpg
    • Customer Story & Case Study

    One Clearlake Centre

    One Clearlake Centre is an 18-story, Class-A commercial office building housing tenants in a variety of industries including financial and legal services, office staffing and insurance. The LEED Silver Certified building is owned by AEW Capital Management, LP and managed by CBRE, Inc., the world’s largest commercial real estate services and investment firm. Committed to sustainability, CBRE was the first company in its industry to achieve carbon neutrality in its operations.

  • Louheed Town Centre hero.JPG
    • Customer Story & Case Study

    Lougheed Town Centre

    Founded in 2005, Shape Properties, a visionary real estate investment and development company based in Vancouver, BC, has become one of the most active fully integrated developers in Western Canada. With a vision of creating vibrant urban lifestyle destinations, Shape Properties dramatically transforms the interaction between living, shopping, dining and entertainment. Driven by the philosophy of creating a dramatically different offering, along with their commitment and passion for client satisfaction, Shape Properties is elevating standards in the commercial real estate sector. The company is currently in the process of developing Lougheed Town Centre, a popular regional shopping center.

  • Delta College.jpg
    • Customer Story & Case Study

    Enhancing Cooling Efficiency at Delta College

    Sustainability-driven college turns to ice-based energy storage and other green technologies to lower energy use and costs; reduces demand by 1.5 MW.