This is the login for Trane® Connect™ and other Trane® commercial applications. Trane® Connect™ is our secure, cloud-based customer portal to access your building systems to remotely monitor and manage building systems, and conduct routine maintenance.
Wellsphere from Trane® is a holistic approach to building wellness. It’s a multi-disciplinary collective of experts using world class technologies and services to improve the viability of your building.
The TCACS is far more than an air filter. It’s a one-of-a-kind blend
of three technologies: filtration, germ-killing ultraviolet light, and
a photocatalytic oxidation (PCO) process.
Neutralize and reduce organic contaminants in your air with the Trane Catalytic Air Cleaning System
Stand in your building’s lobby and take a deep breath. You followed
all building codes. Your ventilation system is bringing outside air
into your building. But does it feel fresh? Is it as clean as you want
it to be?
Outside air can contain contaminants. People bring germs into the
building. And any new furnishings added to the building often
introduce odor and volatile organic compounds (VOCs). Even though your
HVAC system has filters, you may still be circulating germs, viruses,
VOCs and other gases that are too small to be captured. Equipping your
air handler with a Trane Catalytic Air Cleaning System (TCACS) can
help reduce biological organisms such as spores, bacteria and even the
tiniest viruses. It can also reduce irritating odors from organic
compounds such as fumes from paint, glue and cleaning chemicals, and
capture airborne particulates like dust and mold.
Here's How It Works
Air entering the TCACS passes first through a MERV 13 high-efficiency
particulate filter, which captures many of the larger biological
contaminants and small airborne particles such as mold spores and pollen.
Viruses, odors, VOCs and micro-organisms pass through the filter and
into the TCACS’ ultraviolet germicidal irradiation (UVGI) area, where
they are exposed to a high-intensity ultraviolet light. This UV
radiation penetrates microorganisms such as fungi, bacteria and
viruses and damages their DNA bonds, sterilizing them.
As the air is being exposed to UVGI, it’s also passing through a
mesh panel coated with titanium dioxide (TiO2 ). When subjected to
ultraviolet photons, TiO2 creates hydroxyl radicals, one of the most
powerful oxidizing agents in nature. As air passes through this
ultraviolet-powered catalyst, the radicals oxidize gaseous organic
compounds, such as odors and VOCs, reducing them to minute amounts of
harmless carbon dioxide and water. The radicals and UV light work
together to inactivate and decompose organic contaminants.
Services
2018 Trane Brea California 0753_932x932_Services-Operate Maintain and Repair-Rental.jpg
Rental Solutions
Our approach to temporary HVAC and power goes beyond the typical
drop-off. We design, deliver, install and even monitor safe and
efficient rental solutions. Short term, long term, chiller, generator,
or portable AC unit, we have the fleet and people where and when you
need them.