Mansfield Memorial Homes to Complete Energy-Saving Upgrades for a More Sustainable Future
Trane providing efficient systems for the care facility campus
DAVIDSON, N.C., June 17, 2024 – Mansfield Memorial Homes in Mansfield, Ohio will be collaborating with Trane® – by Trane Technologies (NYSE: TT), a global climate innovator, to implement energy efficient upgrades to help reduce rising energy and operational costs while improving resident’s daily experience.
The updates will include the installation of solar panels on each of the care facility’s four buildings. The clean, renewable power generated by these systems will be used to help offset power from the grid and will be a self-sustaining, reliable source of power.
In addition, the care facility will replace the outdated fluorescent lighting systems in it’s four buildings with high-efficiency LED fixtures. In addition to improving light levels and overall aesthetics, the new system includes energy-saving features such as sensors that turn lights on and off as rooms are occupied and dimmers in key areas.
These improvements are expected to save the care facility more than $60,000 in energy and operational costs annually, resulting in up to a 25% reduction in energy consumption and greenhouse gas emissions. The upgrades will begin soon and are expected to complete by the end of the year.
The project will be funded by a $1.35 million grant from the Ohio Department of Development and will also receive tax incentives designed to drive further investment in energy projects.
# # #
About Mansfield Memorial Home
At Mansfield Memorial Homes, we meet the golden era of individual’s life with an enduring commitment, offering superior quality care centrally focused on compassion, dignity, and respect while serving our esteemed residents. Our exceptional memory care facilities are specially designed to cater to the holistic requirements of our residents. Our memory care facility, renowned as a leading senior rehabilitation center in Ohio, comprises a devoted team of proficient nurses. They are well-prepared and committed to providing outstanding, customized care to each resident. The kernel of our services lies in our substantial commitment to the welfare of our residents, ensuring that your loved ones receive unrivaled care rooted in fostering dignity and respect.
About Trane
Trane – by Trane Technologies (NYSE: TT), a global climate innovator – creates comfortable, energy efficient indoor environments for commercial and residential applications. For more information, please visit www.trane.com or www.tranetechnologies.com.
About Trane Technologies
Trane Technologies is a global climate innovator. Through our strategic brands Trane® and Thermo King®, and our portfolio of environmentally responsible products and services, we bring efficient and sustainable climate solutions to buildings, homes and transportation. Visit tranetechnologies.com.
Media Contact:
Barb Bjork
Trane by Trane Technologies
612-598-4492, barb.bjork@tranetechnologies.com