Chiller-Heaters
You may be closer to electrification of heat than you think.
Electrification of heat requires reimagining chillers and thinking differently about applying them to HVAC systems. Trane understands the broad system-wide aspects that are necessary to heat your building, starting with your chiller.
Why choose a chiller-heater?
If you already have a chiller, you may be closer to electrification of heat than you think. Traditionally used for cooling, many chillers are also capable of heating, providing a reliable path to building electrification.
Chillers enabled with heat recovery are extremely energy efficient and provide the first step to electrification of heat. Heat recovery enables chillers that would otherwise reject heat to utilize that energy for heating. Once you have recovered all the heat you can, adding a reversible heat pump to a unit optimizes heating or cooling operation. Multipipe units can provide heating and cooling simultaneously.
Electrification of heat requires reimagining chillers and thinking differently about applying them to HVAC systems. Trane understands the broad system-wide aspects that are necessary to heat your building, starting with your chiller.
Getting off to the right start
The best solution for any building depends on many factors. The first step is to analyze what type of chiller-heater system will deliver the decarbonization outcomes you are seeking. Trane's system experts provide guided expertise at every step: from assessing needs, to implementing the solution, and even validating results

Comprehensive Chiller-Heater Systems
Some system design and control principles from chilled-water systems transfer well when applied to chiller-heater systems. However, there also are some important considerations and differences. Ready to apply chillers to your HVAC system? We’re here to help.
Chillers
Trane has one of the industry’s largest portfolios of chiller-heaters, ranging from 20 to 4,000 tons. Compare heat recovery vs heat pump equipment and learn about their basic functionality here.
Heat Recovery and Heaters
Adding heat recovery to a unit is an efficient and simple way to electrify heat, because heat recovery recycles heat that would normally be wasted in the cooling process and instead uses it to heat the building. Heat recovery units are set to the chilled-water set point. So, as long as there is a demand for cooling, the unit can also provide heat.
When a building is heating dominant, water-cooled chillers may be controlled to the hot-water set point to operate primarily as heaters instead. Water-cooled chillers may also be referred to as heat pumps.
Reversible Heat pumps
A key enabler for decarbonization, Trane heat pumps use a reversing valve to provide electrified heating or cooling. Because they don’t generate heat and simply move heat, they can be up to three times more efficient than other forms of electrified heating.
Simultaneous heating and cooling
Need a multipipe unit that can do both heating and cooling? Trane multipipe units can provide cooling and heating at the same time.
Maximize the benefits over time
Once your Trane Chiller-Heater system is in place, you’ll want to keep the benefits going. Trane’s service organization understands the nuances of electrified system performance, and how to maximize the benefits of your chiller-heater over the long term through professional proactive maintenance and energy monitoring.
Any building can electrify HVAC—and Trane can help
Trane offers a broad range of electrified heating solutions that can help meet your electrification needs. Your local Trane office can help you determine the best combination of technologies to use.

Variable Refrigerant Flow (VRF) systems
Trane® / Mitsubishi Electric VRF Systems consolidate heating and cooling into one all-electric, multi-zone system. VRF is popular for its reduced operational costs and reliable, energy-efficient comfort year-round—even in extremely cold climates. It can also be easily configured for a variety of buildings, new and existing, including offices, hotels, schools, multi-family, and mixed-use spaces.

Packaged Units and Split Systems
For small to mid-sized commercial buildings, Trane has multiple choices. Each delivers efficient and effective heating with integrated heat pumps.